Back to Main Menu

ESRI Integration Configuration

Objective: Gain an understanding of how to integrate Predictor with Esri ArcGIS Online & ArcGIS Enterprise and link to an ArcGIS feature service layer, in order to use ESRI as a data source when importing.

Prerequisites: An Esri ArciGIS Online account or access to a federated Portal for ArcGIS is required in order to integrate with Predictor

Introduction

Predictor provides the ability to integrate directly with Esri ArcGIS Online & ArcGIS Portal (included with ArcGIS Enterprise), which then allows for ESRI to be used as a data source when importing data into Predictor.

Configure Integration

First select the ‘Model’ tab within the Portfolio, and then open the Menu and select ‘Integration from ArcGIS’:

 

This will open the Esri ArcGIS Online & ArcGIS Enterprise Integration Wizard:

 

Click ‘Next’ to proceed to the Configure ArcGIS Feature Services screen. Esri ArcGIS feature services are added to Predictor’s integration, to be later used as publishing destinations for simulation outputs:

 

From this screen, new ArcGIS feature services can be configured for use in Predictor, and existing feature services that have already been configured will appear in the list.

Add new Feature Service Definition

To add a new feature service, click ‘Add Service’, the following sidebar will open:

 

Feature Service Configuration

In the ESRI Service dialog window the following definitions are required:

• Feature Service Name*: A mandatory field to give a name to the feature service, as it will appear in Predictor. This does not need to match the name as it appears in ArcGIS Online.

• Feature Service URL (REST API endpoint)*: A mandatory field to specify the location of the feature service to connect to. This URL comes from within ArcGIS online/ArcGIS Enterprise.

Authentication to ESRI

Typically ArcGIS feature services require authentication in order to connect to them, in which case authentication details must be added to Predictor.

No Authentication option

A publicly shared feature service does not require authentication in order for Predictor to connect to the feature service. For this reason, the 'None' option is provided as an authentication type. It allows Predictor to consume the feature service data as a data source.

ESRI Token

To do this, select ‘Token’ from the Authentication dropdown:

 

Next, click ‘Set Credentials’ to open the enter credentials window:

 

Authentication and token generation can be made using either the user Id and password from the ArcGIS Online account, or by entering an authentication token key.

ESRI User Id and Password

Enter an ESRI username and password for an ESRI user belonging to an ESRI group that has access to the target feature service. If the user Id and password are valid, a token will be generated and used to authenticate to ESRI when accessing the data or publishing simulations.

ESRI Token

The authentication token can be generated using the ArcGIS Online's/ArcGIS Enterprise token page. If using Single Sign On (SSO) first log into your ArcGIS Online/Enterprise environment then open a new browser tab.

 

For ArcGIS Online the default URL is https://www.arcgis.com/sharing/generateToken.

 

For ArcGIS Enterprise the URL is dependent on your Enterprise server host, port, and site name https://<host>:<port>/<site>/sharing/rest/generateToken. In the following example the server host is arcgis106.assetic.office, the port is not defined as it is redirected automatically to the correct port, and the site is 'portal': https://arcgis106.assetic.office/portal/sharing/rest/generateToken

 

When generating the token, the 'Webapp URL' option must be used. The URL to apply for the 'Webapp URL' is the URL already entered as the 'Feature Service URL' in the configuration step above (For example, https://arcgis106.assetic.office/server/rest/services/Hosted/TW_assetic/FeatureServer).

 

Click on the 'Generate Token' button, copy the generated token, and paste into the 'token' box of the Predictor 'Edit Credentials' dialog window.

Test Credentials

ArcGIS Enterprise

For ArcGIS Enterprise the default value for the token URL in the 'Generate Token URL' box must also be modified because this default is for ArcGIS Online. Paste in the same URL as what was used to navigate to the token generation page.

 

Once the credentials or token have been added and the token URL is correct click ‘Test Connection’ to confirm the authentication. The following screenshot is for an ArcGIS Online feature service.

 

Once the connection is working, click ‘Next’ to add the feature service. It will now be visible in the Feature Services list in the Integration Wizard:

Configure Feature Layers

Once the feature service has been added, specific feature layers from that service are added. Select the Feature Service from the list, then click ‘Next’ to proceed to the ‘Configure Layer’ screen:

Add Layer

Click ‘Add Layer’ to add a new feature layer, and the ‘Add Esri Layer’ sidebar will appear, and the list of available Layers will be loaded:

 

Next, select the layer(s) to add to Predictor from the list, and click ‘Save’:

 

The added layer will appear in the list:

 

Click 'Finish' to complete the Integration process.

Additional feature services can be defined by repeating the above steps. This allows different feature service to be used as the data source as needed.